Yes, as long as the wiring is done correctly, there will be no issues.

Questions?
Talk to a specialist
1.877.297.6937
We are having issues with Support Ticket Submissions. Please use the "Let's Chat" or call 1-877-297-6937 to connect with support while we resolve this issue.
—The BAS UPS has 3 outputs, one at 24W and two at 5W. Could the two 5W outputs be wired together in parallel in order to power a device operating at between 5-10W?
1.877.297.6937
© 2025 Cyber Power Systems (USA), Inc. CyberPower is a registered trademark and brand of Cyber Power Systems (USA), Inc. All rights reserved.