Yes, during the setup process you can provide a unique name to identify each UPS system and location.

Questions?
Talk to a specialist
1.877.297.6937
We are having issues with Support Ticket Submissions. Please use the "Let's Chat" or call 1-877-297-6937 to connect with support while we resolve this issue.
—FAQs
1.877.297.6937
Yes, during the setup process you can provide a unique name to identify each UPS system and location.
Using the “Group” function allows you to manage your UPS systems by office location, business, and geographical location.
You cannot perform a UPS system shutdown with PowerPanel Cloud. The app only provides monitoring.
This error message can result from a connection issue or more commonly, the email address was already used to setup an account.
PPB is a new version of CyberPower’s business class monitoring and management software. It has an updated graphical interface, it’s designed to work with future updates of operating systems, and has enhancements to make setting up and use easier.
No, you can only install one version or the other.
Laser printers use a very high amount of power and can easily overload your UPS. Overloads of this type can damage your UPS. As such we ask that you do not plug laser printers in to the battery backed outlets of the UPS.
One CyberPower Surge Protector, one user manual.
Indoor use only.
Computers, home entertainment equipment, cable DSL/modems, phone/fax/modem, cable and satellite boxes, and other electronics you wish to protect.
CyberPower will repair or replace properly connected equipment, under certain terms and conditions, if it is damaged by a power surge.
Shared amperage means multiple ports share the amperage available. Example: If multiple devices are charging at once, each device shares the charging power and can get up to 2.1 amps of the available power depending on the amount amperage available and number of devices that can be connected.
Explore product guides, manuals, publications, and more
Learn more about warranties and register your product
A-to-Z definition guide for common CyberPower phrases and terms
© 2025 Cyber Power Systems (USA), Inc. CyberPower is a registered trademark and brand of Cyber Power Systems (USA), Inc. All rights reserved.