The AVR functionality is only for the Battery/Surge outlets. It will not correct the voltage on the Surge only outlets.

Questions?
Talk to a specialist
1.877.297.6937
We are having issues with Support Ticket Submissions. Please use the "Let's Chat" or call 1-877-297-6937 to connect with support while we resolve this issue.
—FAQs
1.877.297.6937
The AVR functionality is only for the Battery/Surge outlets. It will not correct the voltage on the Surge only outlets.
Category 6 cable, commonly referred to as Cat 6 (Cat6), is a standardized cable for Gigabit Ethernet and other network physical layers. It is backward compatible with the Category 5/5e cable standards.
The M1100XL can have up to two (2) additional battery packs (model BP36V60ART2U) added to it via the connection on the back panel. The M550L and M750L are not equipped for additional batteries.
Category 5 has been superseded by the Category 5e (enhanced) specification. The Category 5e specification improves upon the Category 5 specification by tightening some crosstalk specifications and introducing new crosstalk specifications that were not present in the original category 5 specification. The bandwidth of category 5 and 5e is the same: 100 MHz.
Yes, however, the LCD panel will be easier to use when the UPS is in its standard orientation. If you choose to position the UPS unit in a non-standard position, make sure the fan on the back and at least one of the side vents are left unobstructed so the UPS has plenty of airflow.
Category 5 cable (Cat 5 or Cat5) is a twisted pair cable for carrying signals. This type of cable is used in structured cabling for computer networks such as Ethernet. The cable standard provides performance of up to 100 MHz and is suitable for 10BASE-T, 100BASE-TX (Fast Ethernet), and 1000BASE-T (Gigabit Ethernet). Cat 5 is also used to carry other signals such as telephony and video.
No. A direct USB or serial connection is required to manage this UPS unit with PowerPanel Business software.
Yes. An incorrect voltage might damage the device. Check to make sure that the voltage selector on the Universal Power Adapter is set to the proper voltage for the device you want to connect.
Yes. Desktops, laptops, USB hubs/chargers, phones and other equipment can be connected to this UPS as well. It will provide electricity to them during a power outage just as it would with connected medical equipment.
The voltage required will typically be identified in the device’s user manual and/or on the device itself. If you cannot determine the proper voltage, contact the manufacturer of the device and ask for the information.
No. Our medical-grade UPS units are designed and certified to meet UL 60601-1 requirements for use within patient care vicinities for non-critical care equipment. They have not been designed or certified for use with life support or other critical care equipment and should not be used for that purpose.
The voltage selector supports multiple voltages. The range varies according to the model. CPUAC600: 3V, 4.5V, 6V, 7.5V, 9V, and 12V. CPUAC1U1300: 3V, 4.5V, 5V, 6V, 7.5V, 9V, and 12V. CPUDC1U2000: 3V, 4.5V, 6V, 9V, and 12V.
Explore product guides, manuals, publications, and more
Learn more about warranties and register your product
A-to-Z definition guide for common CyberPower phrases and terms
© 2025 Cyber Power Systems (USA), Inc. CyberPower is a registered trademark and brand of Cyber Power Systems (USA), Inc. All rights reserved.