Two CyberPower UPS Systems Named Best for Gaming by PC Gamer

September 3, 2024 by CyberPower

Cyber Power Systems (USA), Inc. a leader in power protection and power management products, today announced that PC Gamer has named two of its UPS (uninterruptible power supply) systems as top battery backup units for gaming. Based on the publication’s vetting and testing methods, PC Gamer cited the CyberPower CP1500PFCLCD as the best UPS system for most gamers, and the CyberPower EC650LCD as the best UPS system for networking and accessories.

“We are delighted to again receive accolades from PC Gamer for two of our power protection products,” said Brent Lovett, general manager and president of CyberPower. “Gaming enthusiasts are serious about their experience. They need to protect their equipment from outages and power surges to avoid disrupting their progress and damaging their gear.”

The best-selling CyberPower PFC Sinewave CP1500PFCLCD UPS system brings robust power protection in a mini-tower form factor for electronics requiring active PFC (power factor correction) power source compatibility. Its features include a tilting, multi-function color LCD control panel for easy monitoring, and a USB-C charging port for additional devices.

Lovett said: “The CP1500PFCLCD is built with the ideal features for PC gaming: sine wave output for sensitive and advanced gaming hardware as well as a 1500VA rating for larger gaming setups.”

PC Gamer lauded the UPS system as one of the best on the market, offering great value with true sine wave output given most UPS systems in the price range only provide simulated sine-wave output.

Ideal for smaller accessories and networking equipment, PC Gamer recognized the CyberPower EC650LCD UPS system for having excellent battery life for its compact size and 650VA capacity, and an ECO mode for connected equipment. ECO mode is an energy-efficient, user selectable feature for some surge-protected outlets. When the device is off or in sleep mode, the UPS automatically cuts power to computer peripherals connected to any outlets in ECO mode.

Read the full CyberPower UPS reviews at PCGamer.com.

About Cyber Power Systems (USA), Inc.

CyberPower designs and manufactures uninterruptible power supply systems, power distribution units, surge protectors, remote management hardware, power management software, mobile chargers and connectivity products. The company serves customers in enterprise, corporate, government, education, healthcare and small office/home office environments. CyberPower products are available through authorized distributors and sold by value-added resellers, system integrators, managed service providers, select retailers, and online resellers. For more information, visit:
https://wp-dev.cyberpowersystems.com/.

About PC Gamer

PC Gamer is the global authority on PC games, covering the PC gaming industry for more than 20 years. The publication continues that legacy today with worldwide print editions and around-the-clock news, features, esports coverage, hardware testing, and game reviews on PCGamer.com as well as the annual PC Gaming Show at E3.

Contacts
Cyber Power Systems (USA), Inc.
Tim Madsen, 952-403-9500
tim.madsen@cyberpower.com